Configure the main panel (type)

Add and configure a panel loader that defaults to the speed panel.
  1. In
    Project view
    , right-click
    MainPanel (type)
    and select
    New
    Containers
    Panel loader
  2. Hover-over the panel loader, select
    Edit
    , and enter
    MainPanelLoader
    .
  3. In
    Properties
    pane, create a dynamic link between
    Panel
    and
    ProjectName
    UI
    RemotePanels
    SpeedPanel (type)
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal