Types of methods
There are two types of methods -- local and global.
Local methods
Local methods are used in a single project and are defined by object type and their instances.
Acknowledge all
is an example of a local method for an alarm. Objects that define methods include:
- alarms
- logged
- database
- some graphic object
Global methods
Global methods are available in
FactoryTalk Optix Studio
regardless of the project node. Global methods include: - variable
- core
- alarm
- UI
- recipe
Provide Feedback