Backup folders

The backup folder contains one folder for every project.
The default location for the backup folder is:
%localappdata%\Rockwell Automation\FactoryTalk Optix\Studio\Backups\[Project Name]
Each of the project folders consists of other subfolders with these different types of backups:
  • Automatic
    : three backups, performed when saving the project
  • Recovery
    : one backup, performed when a corrupt project is opened and repair attempted in
    FactoryTalk Optix Studio
    . See Restore a project.
  • Upgrade
    : two backups, performed when updating the project to make it compatible with a newer version of
    FactoryTalk Optix Studio
    . 
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal