Event configuration

Configuration of an event type to monitor through Events logger.
BrowseName
EventConfiguration
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Event source
EventSource
Source node of the events of interest. If empty, considers the events of interest generated by any project object.
Listen subtree
MonitorSubtree
If True, sources child nodes of the node selected in Event source.
Event type
EventType
Type of event for which to record the data.
Non-interactive sessions excluded
ExcludeNonInteractiveSessions
Records only the events generated by user interactions with the application graphical interface and ignores events generated by other logics.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.