Onboarding A New User

To onboard user to FactoryTalk Energy Manager, User should have access to the FactoryTalk Energy Manager service and FactoryTalk DataMosaix service. Data scientist role should be assigned in FactoryTalk DataMosaix.
IMPORTANT:
  • FactoryTalk Energy Manager service-level role & FactoryTalk DataMosaix Data scientist role are required for any new user to access the FactoryTalk Energy Manager application.
  • Users already having FactoryTalk Hub organization-level roles can access the FactoryTalk Energy Manager application, but they cannot perform any changes in the user management section of FactoryTalk Hub until or unless they are assigned the FactoryTalk Energy Manager – FactoryTalk DataMosaix service-level roles.
  • If the user has an organization-level role and the FactoryTalk Energy Manager service-level role, still they require the FactoryTalk DataMosaix Data Scientist role to access the FactoryTalk Energy Manager application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal