Configure Virtual Meter and Tag Mapping

Perform the following steps to configure
Virtual meter
formula and tag mapping:
  1. Under the
    Configuration
    tab, click
    Edit
    and then click on
    Variable
    .
    The
    Variable Configuration
    dialog is displayed.
    Virtual Meter Dashboard
  2. Provide the
    Variable Name
    .
  3. Under
    Select Meter
    section, select the
    Resource meter
    with same
    Resource Type
    ,
    Measurement (Consumption/Demand)
    , and under the same
    Site/Area/Work Center
    .
    Variable Configuration Dialog
  4. Click
    Submit
    .
  5. Click the [] icon to add another variable.
    NOTE:
    • If another variable is not added after the icon,
      Invalid Formula
      is displayed.
    • Same
      Resource meter
      cannot be added twice for the same
      Virtual meter
      .
  6. When more than two variables are added,
    Valid Formula
    is displayed.
    Virtual Meter Configuration (Continued)
  7. Click
    Save
    .
  8. The User can edit/delete any variable and add a new variable.
IMPORTANT:
  • Maximum of five variables can be added while configuring the formula for the
    Virtual meter
    .
  • Maximum of five virtual meters can be added under any
    Site/Area/Work Center
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal