Add Virtual Meter

Perform the following steps to add a
Virtual meter
to the hierarchy list:
  1. Select
    Site
    or
    Area
    or
    Work center
    from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    The
    Add Component
    dialog box is displayed.
  3. Under
    Meter
    from the left pane, select
    Virtual meter
    and set these parameters:
    • Resource Type
      : Select a resource type from the drop-down list.
    • Measurement
      : Select a measurement from the drop-down list.
    • Name
      : Provide a virtual meter name.
    • Description
      : Provide a description of the virtual meter.
  4. Click
    Add
    .
    Add Virtual Meter
    Add Virtual Meter (Continued)
    The "
    Virtual meter added under Site or Area or Work center or Work units successfully
    " message is displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal