Add Resource Meter

Perform the following steps to add the Resource Meter to the hierarchy list:
NOTE:
The following point is required to view data on
Resource meter dashboard
:
  • Default unit should be configured for demand and consumption measurement with correct tag mapping.
  1. Select the
    Site
    or
    Area
    or
    Work center
    , or
    Work units
    from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    The
    Add Component
    dialog box is displayed.
  3. Under
    Meter
    from the left pane, select
    Resource
    and set these parameters:
    • Resource Type
      : Select a type of resource from the drop-down list.
      Resource Meter Types
      NOTE:
      • The resource types that are configured under the default units are displayed in all resource type drop-down.
      • The units drop-down to display only valid resource type units associated with the selected resource type.
    • Name
      : Provide a Resource meter name.
    • Description
      : Provide a description of the Resource meter.
  4. Click
    Add
    .
    Add Resource Meter
The "
Resource meter added under Site or Area or Work center or Work units successfully
" message is displayed.
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal