Add Production Meter

Perform the following steps to add the
Production Meter
to the hierarchy list:
NOTE:
The following point is required to view data on
Production meter dashboard
:
  • Correct tag mapping should be done for production count measurement.
  1. Select
    Site
    or
    Area
    or
    Work center
    , or
    Work units
    from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    The
    Add Component
    dialog box is displayed.
  3. Under
    Meter
    from the left pane, select
    Production
    and set these parameters:
    • Name
      : Provide a production meter name.
    • Description
      : Provide a description of the production meter.
  4. Click
    Add
    .
    Add Production Meter
The "
Production meter added under Site or Area or Work center or Work units successfully
" message is displayed.
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal