Add Process Value Meter

Perform the following steps to add a
Process value meter
to the hierarchy list:
NOTE:
The following point is required to view data on
Process value meter dashboard
:
  • Correct tag mapping should be done for the respective process value attributes.
  1. Select
    Site
    or
    Area
    or
    Work center
    , or
    Work units
    from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    The
    Add Component
    dialog box is displayed.
  3. Under
    Meter
    from the left pane, select
    Process value
    and set these parameters:
    • Name
      : Provide a process value meter name.
    • Description
      : Provide a description of the process value meter.
  4. Click
    Add
    .
    Add Process Value Meter
The "
Process value meter added under Site or Area or Work center or Work units successfully
" message is displayed.
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal