Audience
This document shall be utilized following the successful installation of the FactoryTalk Edge node. Installation instructions are provided within the box. This quick start guide provides necessary instructions for connecting the edge node to the local network along with onboarding within FactoryTalk Edge Manager user interface. After successful completion of onboarding the edge node, users should reference the FactotyTalk Edge Manager User Guide linked at the bottom of the manual.
Provide Feedback