Install the Device
- Unbox and install the Edge Node device as per the instructions given within the ASEM 6300B Box PCs document.
- Connect an Ethernet cable from portEth1on the Edge node to a managed switch.NOTE:Ensure the managed switch has access to a DHCP server along with an active path to the Internet for HTTPS traffic.NOTE:If a DHCP server is not present on-site, follow the link below to set a static IP address for the edge node: https://help.zededa.com/hc/en-us/articles/8341291771419-EVE-Network-Bootstrap
Provide Feedback