Configure general controller settings

Use the
Controller
-
General
page to configure the following settings:
  • Communication
    -
    Timeout
    : Sets the communication timeout period between 300 milliseconds and 15000 milliseconds. The default value is 3000 milliseconds.
  • Data Log
    -
    ZIP file folder hierarchy
    : Specifies whether to reserve the folder structure of the data log files or combine data log files to a TXT file when exporting data logs. The default setting is
    Preserve source folder structure
    .
  • Recipe
    -
    Destination
    : Defines the destination path on your computer for uploading recipes from the SD card. The default path is the Downloads folder.
To configure general controller settings
  1. From the
    File
    menu, select
    Settings
    .
  2. In
    Settings
    , select
    Controller
    General
    .
  3. Customize the settings as needed, and then select
    OK
    .
    Select
    Reset
    to restore the default settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal