Rename a controller

Use the
Properties
pane to rename a controller.
Naming conventions are as follows:
  • The name can contain up to 32 characters.
  • The name is restricted to alphanumeric characters and underscores.
  • The name cannot end with an underscore or contain consecutive underscores.
To rename a controller
  1. In
    Project Organizer
    , select the controller.
    The
    Properties
    pane displays the controller name and catalog ID.
  2. In the
    Properties
    pane, enter the new name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal