Delete a controller

When a controller is deleted from a project, the action is not reversible. All logic programs, variables, and user-defined function blocks associated with the controller are deleted.
To delete a controller
  1. Open
    Delete Devices
    by doing one of the following:
    • In
      Project Organizer
      , right-click the controller, and then select
      Delete
      .
    • In
      Project Organizer
      , select the controller node, and then select Delete device button.
    • In
      Project Organizer
      , select the controller, and then select the
      Delete
      key.
  2. In
    Delete Devices
    , select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal