Commands in structured text editor

This section introduces the commands when you right-click the language editor or the scroll bar.
Commands in structured text editor
Command
Description
Cut
Moves the selected text or the current line to the clipboard.
Copy
Copies the selected text or the current line to the clipboard.
Paste
Inserts the clipboard text to the current cursor position.
Add element
Opens
Toolbox
if hidden, highlighting your last position.
Create new variable
Opens
New variable
to define a new variable within the code.
Find all references
Opens the cross-reference browser to view reference information of the selected variable.
Select variable
Opens the variable selector to replace the selected variable with a new one.
Open instruction parameters
Opens the local variable grid to view the variables that are used in the selected instruction.
Open instruction logic
Opens the definition of the selected instruction.
Open monitor
Opens the corresponding variable grid to monitor the variable in real time. The menu is available when the controller is online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal