WHILE statement

This section is about the WHILE statement syntax and examples.
IMPORTANT: Input variables are not refreshed during WHILE iterations. The state change of an input variable cannot be used to describe the condition of a WHILE statement. Using an input variable in this manner might cause unexpected controller behavior.
WHILE statement properties
Item
Description
Name
WHILE ... DO ... END_WHILE
Meaning
Iteration structure for a group of ST statements.
The "continue" condition is evaluated before every iteration.
Syntax
WHILE <Boolean_expression> DO <statement> ; <statement> ; ... END_WHILE ;

Example

(* ST program using WHILE statement *) (* this program uses specific "C" functions to read characters *) (* on a serial port *) str := ''; (* empty string *) nbchar := 0; WHILE ((nbchar < 16) & ComIsReady ( )) DO str := str + ComGetChar ( ); nbchar := nbchar + 1; END_WHILE;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal