Expressions and parentheses

Structured text (ST) expressions consist of operators and their operands. An operand might be a constant (literal) value, a control variable, or another expression (or sub-expression).
For each single expression, which combines operands with one ST operator, the type of the operands must match. A single expression has the same data type as its operands and can be used in a more complex expression.

Example 1

ST expression examples
Example
Result
(boo_var1 AND boo_var2)
BOOL type
not (boo_var1)
BOOL type
(sin (3.14) + 0.72)
REAL type
(t#1s23 + 1.78)
Invalid expression
Parentheses are used to isolate subcomponents of an expression and to explicitly order the priority of operations. When no parentheses are given for a complex expression, the operation sequence is implicitly given by the default priority between the ST operators.

Example 2

ST expression examples
Example
Result
Description
2 + 3 * 6
Equals 2+18=20
Multiplication operator has a higher priority
(2 + 3) * 6
Equals 5*6=30
Expressions in parentheses take precedence
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal