Call functions

The structured text programming language can call functions. Function calls can be used in any expressions, and contain properties explained in the following table.

Function call properties

A function is an instruction block that has input parameters and one output parameter. It can be written in structured text (ST), ladder diagram (LD), or function block diagram (FBD) languages.
Properties of function calls
Property
Description
Name
The name of the called function written in an IEC 61131-3 language.
Meaning
Calls an ST, LD, or FBD function, and gets its return value.
Syntax
<variable> := <funct> (<par1>, ... <parN>);
Operands
The type of return value and calling parameters must follow the interface defined for the function.
Return value
Value returned by the function.
Function call example
Function call example
When setting the value of the return parameter in the body of a function, you can assign the return parameter using the same name as the function:
FunctionName := <expression>;

Example: IEC 61131-3 function call

(* Main ST program *) (* gets an integer value and converts it into a limited time value * appl_timer := ANY_TO_TIME (ana_timeprog * 100); (* Called FBD function named 'SPlimit' *)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal