Go to a rung in the ladder editor

Use the
Go to Rung
dialog in the ladder editor to jump to a specific rung quickly within a ladder Program Organization Unit.
To go to a rung in the ladder editor
  1. In the ladder editor, select Go to rung icon to open
    Go to Rung
    .
  2. In
    Go to Rung
    , enter the rung number or use the arrow buttons (Up triangle icon or Down triangle icon) to select the desired rung number.
  3. Select
    Go
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal