Add a rung to the ladder diagram program

Rungs are graphic components of ladder diagram (LD) programs and represent a group of circuit elements that activate a coil.
To add a rung to the ladder diagram program
  • Do one of the following:
    • From
      Toolbox
      , drag Add rung button to a valid location in the language editor.
      A green dot indicating the valid dropping location indicates a valid dropping location.
    • In the LD language editor, right-click the
      End
      rung, and then select
      Add element
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal