Delete ladder diagram branches or branch levels

Delete a ladder diagram (LD) branch or branch level to remove the branch or branch level and its content from a rung.
To delete LD branches or branch levels
  • Do one of the following:
    • Select the left rail of the branch or branch level, and then select the
      Delete
      or
      Backspace
      key.
    • Right-click the left rail of the branch or branch level, and then select
      Delete
      .
    • Select the right rail of two or more branches or branch levels that are of the same level, and then select the
      Delete
      or
      Backspace
      key to delete them.
    • Right-click the right rail of two or more branches or branch levels that are of the same level, and then select
      Delete
      to delete them.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal