Add a ladder diagram branch level

Instructions placed in a branch level direct the Program Organization Unit to execute the instruction in the current branch level or the instructions in other branch levels.
To add a ladder diagram branch level
  • From
    Toolbox
    , drag Add parallel rung button to a valid location to add a parallel rung.
    A green dot indicating the valid dropping location indicates a valid dropping location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal