Re-order elements in function block diagram programs

In the function block diagram (FBD) language editor, move elements to change the execution order.
To re-order elements in FBD programs
  • Do one of the following:
    • Drag an individual element to the new location. Connections will re-organize when the mouse is released.
    • Use the
      CTRL
      or
      Shift
      key, or drag the cursor to select several elements, and then drag the selected elements or the selection area to the new location. Connections will re-organize when the mouse is released.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal