Instruction blocks in function block diagram programs

The
FactoryTalk Design Workbench
instruction set includes instruction blocks in compliance with IEC 61131-3. Instruction blocks collectively include function blocks, functions, and operators.
Connect instruction block inputs and outputs to variables or other instruction block inputs and outputs.

Instruction block conventions

The IEC61131-3 programming language specification addresses numerous aspects of programmable controllers, including operating system execution, data definitions, programming languages, and instruction sets. The IEC61131-3 specification provides a minimum set of functionalities that can be extended to meet end user applications.

Instruction block names

Functions and function blocks are represented by a box that displays the name of the instruction and the short version of the parameter names. For function blocks with an instance, the instance name is displayed below the function block name.

Instruction block return parameters

  • The return parameter of a function has the same name as the function. The return parameter is the only output.
  • The return parameters of a function block can have any name. Multiple return parameters can provide multiple outputs.
  • You can define the parameters of programs for each controller by navigating the tabs for individual controllers displayed in the
    Parameter
    view.

Instruction block loops

For loops in instruction blocks, because they are initialized with a value, you must use local variables. The following FBD program shows a valid loop where:
  • The local variables initialize both inputs of the greater than or equal operator (>=) and one input of the first AND operator.
  • The output of the second AND operator initializes the second input of the first AND operator.
Instruction block loops
Instruction block loops
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal