Execution rules

Executing a control application for a resource follows eight main steps within a loop. The duration of this loop is defined as the cycle timing for a resource.
  1. Scan input variables
  2. Consume bound variables
  3. Execute Program Organization Units (POU)
  4. Produce bound variables
  5. Update output variables
  6. Save retained values
  7. Process IXL messages
  8. Sleep until next cycle
Execution rules
A diagram showing the execution process of a control application for a resource
In a case where bindings are defined, variables consumed by a resource are updated after the inputs are scanned and the variables produced for other resources are sent before updating outputs.
When a cycle timing is specified, a resource waits until this time has elapsed before starting executing a new cycle. The POU execution time varies depending on the number of active steps in sequential function chart (SFC) programs and instructions such as jumps, IFs, and returns. When a cycle exceeds the specified time, the loop continues to execute the cycle but sets an overrun flag. In such a case, the application no longer runs in real time.
When a cycle time is not specified, a resource performs all steps in the loop, and then restarts a new cycle immediately.
All digital output variables driven by the I/O scan are cleared on a power-up or when transitioning to Run.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal