SIN (sine)
The SIN instruction calculates the sine of a Real value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.SIN

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
|
IN | Input | REAL | Any Real value. |
SIN | Output | REAL | Sine of the input value (in set [-1.0 .. +1.0]). |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. |
SIN examples
SIN function block diagram example

SIN ladder diagram example

SIN structured text example

(* ST Equivalence: *) sine := SIN (angle); result := ASIN (sine); (* result is equal to angle *)
Results

Provide Feedback