COS_LREAL (cosine Long Real)

The COS_LREAL instruction calculates the cosine of a Long Real value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
COS_LREAL
COS_LREAL
COS_LREAL parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
When set to true, the instruction is enabled.
  • TRUE: Execute the current computation.
  • FALSE: There is no computation.
Applies to ladder diagram programs.
IN
Input
LREAL
Any Long Real value.
COS_LREAL
Output
LREAL
Cosine of the input value (in set [-1.0 .. +1.0]).
ENO
Output
BOOL
Enables output. Applies to ladder diagram programs.

COS_LREAL examples

COS_LREAL function block diagram example
COS_LREAL function block diagram example
COS_LREAL ladder diagram example
COS_LREAL ladder diagram example
COS_LREAL structured text example
COS_LREAL structured text example
(* ST Equivalence: *) cosine := COS_LREAL (angle); result := ACOS_LREAL (cosine); (* result is equal to angle *)
Results
Results
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal