ASIN_LREAL (arcsine Long Real)
The ASIN_LREAL instruction calculates the arc-cosine of a Long Real value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.ASIN_LREAL

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
|
IN | Input | LREAL | The value must be within [-1.0 .. +1.0]. |
ASIN_LREAL | Output | LREAL | Arc-cosine of the input value (in set [0.0 .. PI]) = 0.0 for invalid input. |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. |
ASIN_LREAL examples
ASIN_LREAL function block diagram example

ASIN_LREAL ladder diagram examples

ASIN_LREAL structured text examples

(* ST Equivalence: *) cosine := COS_LREAL (angle); result := ACOS_LREAL (cosine); (* result is equal to angle *)
Results

Provide Feedback