SYS_INFO
The SYS_INFO instruction reads the status data block for the
Micro800
controller.Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.SYS_INFO

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL | Instruction block enable.
|
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
SYS_INFO examples
SYS_INFO function block diagram example

SYS_INFO ladder diagram example

SYS_INFO structured text example

Results

Provide Feedback