AFI (always false)

Use the AFI instruction at the beginning of a rung to temporarily disable the rung when debugging without having to delete the rung from the program. Output of this instruction is always FALSE.
AFI
AFI
Language supported: ladder diagram.
This instruction applies to the
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal