SCL instruction timing diagrams examples

The following timing diagram examples describe execution scenarios for the SCL (scaler with alarm) instruction.

Successful SCL execution

Successful SCL execution
Successful SCL execution
Scan cycle description
Scan Cycle
Description
1
When Enable is set to TRUE and input parameters are valid and within range, the Function Block execution starts.
  • Done and EnableOut are set to TRUE.
  • Out is calculated as per given inputs.
  • MaxAlarm, MinAlarm, and Error are set to FALSE.
  • Status ErrorID and are set to 0, because there is no error generated.
2, 3
No change in rung condition.
4
When Enable is set to FALSE, function block execution stops.
  • Done, EnableOut and Error are set to FALSE.
  • ErrorID is set to 0.
  • Out, MaxAlarm, MinAlarm, and Status keep their last value.
5, 6, 7
No change in rung condition.
8
  • When Enable is set to TRUE and input parameters are valid and within range, the function block execution starts.
  • Done and EnableOut are set to TRUE.
  • Out is calculated as per given inputs.
  • MaxAlarm, MinAlarm, and Error are set to FALSE.
  • ErrorID and Status are set to 0, because there is no error generated.
9
When Enable is set to FALSE, function block execution stops.
  • Done, EnableOut and Error are set to FALSE.
  • ErrorID is set to 0.
  • Out, MaxAlarm, MinAlarm and Status keep their last value.
10, 11
No change in rung condition.

Failed SCL execution

Failed SCL execution
Failed SCL execution
In this example, all the input parameters are valid and within range, but InRawMin >= InRawMax. In Scan Cycle 1 and 8, when Enable is set to TRUE and the function block execution starts, Error is set to True and ErrorID is set to 1.

Generation of MaxAlarm

Generation of MaxAlarm
Generation of MaxAlarm
In Scan Cycle 8 of this example, all the input parameters are valid and within range, but In > InRawMax. When Enable is set to TRUE and the function block execution starts, MaxAlarm is set to TRUE.

Generation of MinAlarm

Generation of MinAlarm
Generation of MinAlarm
In Scan Cycle 8 of this example, all the input parameters are valid and within range, but In < InRawMin. When Enable is set to TRUE and the function block execution starts, MinAlarm is set to TRUE.

Output overflow condition and input configuration error

Output overflow condition and input configuration error
Output overflow condition and input configuration error
In Scan Cycle 3 of this example, function block input parameters are valid and within the range, but Out is overflowed because of input parameters. EnableOut is set to FALSE. Out value is invalid.
In Scan Cycle 8 of this example, function block input parameters are valid and within the range, but Out is overflowed because of input parameters and InRawMin >= InRawMax, Error is set to TRUE. ErrorID is set to 1 and Status is set to 3.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal