Use auto-tune with the IPIDController function block

Use the AutoTune parameter of the IPIDController function block to implement auto-tuning in the control program.
Auto-tuning requirements and recommendations
The following is a summary of requirements and recommendations for implementing successful auto-tuning.
  • Autotuning must cause the output of the control loop to oscillate, which means the IPIDController must be called frequently enough to adequately sample the oscillation.
  • The IPIDController instruction block must be executed at a relatively constant time interval.
  • Configure the scan time of the program to be than half of the oscillation period.
  • Consider using a Selectable Timed Interrupt (STI) instruction block to control the IPIDController instruction block.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal