COP string array example

The following example shows a COP (copy) instruction copying a string array into Usint array. The COP instruction skips all the elements in the source array with Zero length.
For this example:
  • Length is specified as 4 bytes.
  • Number of Destination Elements to copy is 4 bytes.
  • All the array elements with Zero length (blanks) are skipped.
  • The COP instruction finds a non zero length element in the string array[1], which is copied into the designation Usint array[1] with 1. One is the length of the string in String array[1]) and Usint array[2] is 65, which is the ASCII code of "A".
  • The COP instruction finds a non zero length element in String array[10] which is "a", which is copied into destination Usint array[3] with 1. One is the length of string in String array[10]) and Usint array[4] is 97 which is ASCII code of "a".
Ladder diagram
Ladder diagram
Array elements with values
Array elements with values
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal