MC_Reset (motion control reset)

The MC_Reset instruction transitions the axis state from Error Stop to Standstill by resetting all internal axis-related errors. The outputs of the function block instances are not changed.
Operation details:
  • If the axis alarm state is not changed after executing MC_Reset, execute MC_Power followed by MC_Reset.
  • MC_Reset only resets the axis state from Error Stop to Standstill. Executing MC_Reset when the axis is in other states, including Disabled, results in an error, and has no impact on ongoing motion or the status of the axis.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro850
L50E and
Micro870
L70E controllers that support motion control.
MC_Reset
MC_Reset
MC_Reset parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
Instruction block enable.
  • TRUE: Execute current MC_Reset computation.
  • FALSE: There is no computation.
Applies only to ladder diagram programs.
AxisIn
Input
AXIS_REF
FB_AXIS_REF
Use the AXIS_REF data type to define AxisIn.
For FB_Axis (feedback axis), use the FB_AXIS_REF data type to define AxisIn.
Execute
Input
BOOL
TRUE: Resets the axis to the rising edge.
ENO
Output
BOOL
Enable output.
Applies only to ladder diagram programs.
Axis
Output
AXIS_REF
Axis output is read-only in ladder diagram programs.
Done
Output
BOOL
TRUE: Axis state is Standstill or Disabled.
Busy
Output
BOOL
TRUE: The function block is not finished.
Error
Output
BOOL
Indicates that an error occurred.
  • TRUE: An error is detected.
  • FALSE: No error.
ErrorID
Output
UINT
A unique numeric that identifies the error. The errors for this instruction are defined in Motion control function block error IDs.

MC_Reset examples

MC_Reset function block diagram example
MC_Reset ladder diagram example
MC_Reset ladder diagram example
MC_Reset structured text example
MC_Reset structured text example
Results
Results
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal