MC_WriteParameter (motion control write parameter)
The MC_WriteParameter parameter modifies the value of a vendor-specific parameter of type REAL.
The parameters set by the MC_WriteParameter function block are only applied to the application temporarily. They are overwritten by the permanent settings, which are configured by the user in
FactoryTalk Design Workbench
motion configuration, when the controller is switched from Program
to Run
, or when the controller power is cycled OFF and ON.Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro850
L50E and Micro870
L70E controllers that support motion control.MC_WriteParameter

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | Instruction block enable.
Applies only to ladder diagram programs. |
AxisIn | Input | AXIS_REF FB_AXIS_REF | Use the AXIS_REF data type to define the parameters for AxisIn. For a feedback axis, use the FB_AXIS_REF data type to define the parameters for AxisIn. |
Execute | Input | BOOL | TRUE: Writes the value of the parameter at the rising edge. |
ParameterNumber | Input | DINT | Parameter identification. The parameter number is defined in Motion control function block parameter details. |
Value | Input | REAL | New value of the specified parameter. |
MC_ExecutionMode | Input | SINT | Values are:
When (MC_ExecutionMode = 0), for all parameters except Duty Cycle (1005), this FB can be completed successfully only when the axis state is Disabled or Standstill. When (MC_ExecutionMode = 0), for Parameter Duty Cycle (1005), this FB can be completed successfully except the axis is in Homing or Error Stop state. For (MC_ExecutionMode = 1), this function block can be successfully completed only when the axis state is Disabled, Standstill, or the ongoing motion can complete, ending with Standstill state. Other input values are reserved currently and are considered as invalid parameters. |
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
Axis | Output | AXIS_REF | Axis output is read-only in ladder diagram programs. |
Done | Output | BOOL | TRUE: The parameter was successfully written. |
Busy | Output | BOOL | TRUE: Indicates that the function block has control of the axis. |
Error | Output | BOOL | Indicates that an error occurred.
|
ErrorID | Output | UINT | A unique numeric that identifies the error. The errors for this instruction are defined in Motion control function block error IDs. |
MC_WriteParameter examples
MC_WriteParameter function block diagram example

MC_WriteParameter ladder diagram example

MC_WriteParameter structured text example

Results

Provide Feedback