MC_ReadParameter (motion control read parameter)

The MC_ReadParameter instruction returns the value of a vendor specific parameter in a Real data type.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro850
L50E and
Micro870
L70E controllers that support motion control.
MC_ReadParameter
MC_ReadParameter parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
Instruction block enable.
  • TRUE: Execute current MC_ReadParameter computation.
  • FALSE: The Value output is reset to 0.
Applies only to ladder diagram programs.
AxisIn
Input
AXIS_REF
FB_AXIS_REF
Use the AXIS_REF data type to define AxisIn.
For FB_Axis (feedback axis), use the FB_AXIS_REF data type to define AxisIn.
Enable
Input
BOOL
  • TRUE: Get the value of the parameter number continuously.
  • FALSE: The Value output is reset to 0.
ParameterNumber
Input
DINT
Parameter identification.
Parameter numbers definitions are defined in motion control function block parameter numbers.
ENO
Output
BOOL
Enable output.
Applies only to ladder diagram programs.
Axis
Output
AXIS_REF
Axis output is read-only in ladder diagram programs.
Valid
Output
BOOL
  • TRUE: Valid outputs are available.
  • FALSE: Valid outputs are unavailable.
Busy
Output
BOOL
  • TRUE: The function block is working and new output values are expected.
  • FALSE: The function block is idle.
Error
Output
BOOL
Indicates an error occurred.
  • TRUE: An error is detected.
  • FALSE: No error.
ErrorID
Output
UINT
A unique numeric that identifies the error. The errors for this instruction are defined in Motion control function block error IDs.
Value
Output
REAL
Value of the specified parameter in the data type, as specified by the vendor.

MC_ReadParameter examples

MC_ReadParameter function block diagram example
MC_ReadParameter function block diagram example
MC_ReadParameter ladder diagram example
MC_ReadParameter ladder diagram example
MC_ReadParameter structured text example
MC_ReadParameter structured text example
Results
Results
Axis monitoring
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal