MC_ReadBoolParameter (motion control read BOOL parameter)
The MC_ReadBoolParameter instruction returns the value of a vendor-specific parameter of type BOOL.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro850
L50E and Micro870
L70E controllers that support motion control.MC_ReadBoolParameter

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | Instruction block enable.
Applies only to ladder diagram programs. |
AxisIn | Input | AXIS_REF FB_AXIS_REF | Use the AXIS_REF data type to define AxisIn. For FB_Axis (feedback axis), use the FB_AXIS_REF data type to define AxisIn. |
Enable | Input | BOOL |
|
ParameterNumber | Input | DINT | Parameter identification. Parameter numbers definitions are defined in motion control function block parameter numbers. |
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
Axis | Output | AXIS_REF | Axis output is read-only in ladder diagram programs. |
Valid | Output | BOOL |
|
Busy | Output | BOOL |
|
Error | Output | BOOL | Indicates that an error occurred.
|
ErrorID | Output | UINT | A unique numeric that identifies the error. The errors for this instruction are defined in Motion control function block error IDs. |
Value | Output | BOOL | Value of the specified parameter in the data type, as specified by the vendor. |
MC_ReadBoolParameter examples
MC_ReadBoolParameter function block diagram example

MC_ReadBoolParameter ladder diagram example

MC_ReadBoolParameter structured text example

Results

Provide Feedback