Example: How to configure Modbus communication to read from and write to a drive

These examples describe how to configure Modbus communication to read status data from and write control data to a
PowerFlex
4 drive using the MSG_MODBUS instruction.

Micro850 L50E wiring

This example uses a
Micro850
L50E controller with a SERIALISOL module plugged into the first slot (Channel 5). A single
PowerFlex
40 is connected, but the diagram below shows how to wire for multi-drop. Refer to the user manual for additional wiring information.
Micro850 L50E wiring
Micro850 L50E wiring

Modbus Read example

The following MSG_MODBUS instruction can be used to read status data from the
PowerFlex
40 drive.
MSG_MODBUS instruction read example
MSG_MODBUS instruction read example
Drive status
An "1807" indicates the drive is:
  • Ready (bit 0 ON)
  • Active (bit 1 ON)
  • Commanded Forward (bit 2 ON)
  • Rotating Forward (bit 3 ON)
  • Status of some digital inputs on the drive
A "278" indicates 27.8Hz.
Refer to the
PowerFlex
user manual for additional information about Logic Status word bits, error code descriptions, commanded and actual speeds, and other status codes.

MSG_MODBUS Read configuration

The following image shows the variable options for the MSG_MODBUS instruction block used to read status data from a
PowerFlex
40 drive.
Variable options for MSG_MODBUS to read status data from a PowerFlex 40 drive
Image showing the variable options for MSG_MODBUS to read status data from a PowerFlex 40 drive

MSG_MODBUS Read variables

The following table identifies the variables and the values used to configure the MSG_MODBUS instruction to read status data from a
PowerFlex
4 drive.
MSG_MODBUS variables and values
Variable
Value
Description
*.Channel
5
Channel 5 - location of SERIALISOL module
*.TriggerType
0
Trigger on False-to-True transition
*.Cmd
3
Modbus Function Code "03" - Read Holding Registers
*.ElementCnt
4
Length
*.Addr
8449
PowerFlex
Logic Status word address + 1
*.Node
2
PowerFlex
Node address
*_laddr[1]
data
PowerFlex
Logic Status word
*_laddr[2]
data
PowerFlex
Error Code
*_laddr[3]
data
PowerFlex
Commanded Speed (Speed Reference)
*_laddr[4]
data
PowerFlex
Speed Feedback (Actual Speed)

MOVE instruction example

The following image shows an example of using the MOVE instruction to move the *_l[1] array value to a Word, which allows you to directly access the individual bits.
MOVE instruction example
MOVE instruction example

Modbus Write example

The following MSG_MODBUS instruction is used to write control data to a
PowerFlex
40 drive.
Modbus Write example
Modbus Write example

MSG_MODBUS Write configuration

The following image shows the variables and the values used to configure the MSG_MODBUS instruction to write control data to a
PowerFlex
4 drive.
MSG_MODBUS Write configuration
MSG_MODBUS Write configuration

MSG_MODBUS Write variables

The following table lists the variables, values, and describes the purpose of each variable.
Write variables
Variable
Value
Description
*.Channel
5
Channel 5 - location of SERIALISOL module
*.TriggerType
0
Trigger on False-to-True transition
*.Cmd
16
Modbus Function Code "16" - Write Holding Registers
*.ElementCnt
2
Length
*.Addr
8193
PowerFlex
Logic Status word address + 1
*.Node
2
PowerFlex
Node address
*_laddr[1]
data
PowerFlex
Logic Command word
*_laddr[2]
data
PowerFlex
Speed Reference word
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal