Validate the IP configurations in Controller B

Use the following steps to verify that the IP settings are correct in Controller B.
To validate the IP configurations in Controller B
  1. In
    Project Organizer
    , double-click the controller to open the controller workspace.
  2. In the
    Controller
    tree, select
    Ethernet
    .
  3. On the Ethernet port configuration page, verify that the IP address settings are correct as identified in the following table.
    IP configurations for Controller B
    IP Configuration Option
    Value
    IP address
    192.168.1.19
    Subnet mask
    255.255.255.0
    Gateway address
    192.168.1.1
The IP address options on your controller configuration page look similar to the following image:
IP configurations for controller B
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal