Review the complete program results

The following example shows the complete MSG_CIPSYMBOLIC messaging program after it has executed.
Global variable grid of the MSG_CIPSYMBOLIC messaging program
Global variable grid of the MSG_CIPSYMBOLIC messaging program
Ladder diagram of the MSG_CIPSYMBOLIC messaging program
 Ladder diagram of the MSG_CIPSYMBOLIC messaging program

Controller B results

The following two images show the values for Controller B before and after the messaging program is executed.
  • Before the program executes
    Global variable grid of the MSG_CIPSYMBOLIC messaging program before execution
  • After the program executes
    Global variable grid of the MSG_CIPSYMBOLIC messaging program after execution
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal