Create global variables for Controller B

Use the following steps to create global variables for Controller B.
To create global variables for Controller B
  1. In
    Project Organizer
    , double-click
    Global Variables
    to open the global variable gird.
  2. In the global variable grid, in the empty row, enter the variable name
    UDINT_FromA
    .
  3. Configure the remaining parameters.
    1. Verify that the data type is
      UDINT
      .
    2. Verify that the
      Read/Write
      attribute is selected.
The global variable gird looks similar to the following image:
Controller B global variable
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal