Message execution process (Rung = TRUE)

The process diagram describes the message instruction events that occur when the Rung condition is True.
Message execution process
Process diagram showing the message execution process when the rung condition is true
  • Com Queue: Message requests added to the Com Queue have a buffer allocated and processed by the communication task. The queue size limit is 4.
  • Wait Queue: Messages that cannot be added to the Com Queue are added to the Wait Queue to be processed at a later time. The Wait Queue does not have a size limit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal