MSG_CIPGENERIC (common industrial protocol generic message)
The MSG_CIPGENERIC instruction sends a common industrial protocol (CIP) explicit message over an Ethernet channel or a serial port.
A maximum of four message requests per channel can be processed in one scan. For ladder diagram programs, message requests are executed at the end of a ladder scan.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro820
L20E,
Micro850
L50E, and Micro870
L70E controllers.MSG_CIPGENERIC

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
IN | Input | BOOL | Rung input state.
|
CtrlCfg | Input | CIPCONTROLCFG | The instruction block execution control configuration. Use the CIPCONTROLCFG parameters to define CtrlCfg. |
AppCfg | Input | CIPAPPCFG | CIP service and application path (EPATH) configuration. Use the CIPAPPCFG parameters to define AppCfg. |
TargetCfg | Input | CIPTARGETCFG | Target device configuration. Use the CIPTARGETCFG parameters to define TargetCfg. |
ReqData | Input | USINT[1..1] | CIP message request data. The array size should be greater than the ReqLength size. |
ReqLength | Input | UINT | CIP message request data length: 0–490. |
ResData | Input | USINT[1..1] | CIP message response data. The array size should be greater than the ReqLength size. When an MSG is triggered or re-triggered, data in the ResData array is cleared. |
Q | Output | BOOL | Outputs of this instruction are updated asynchronously from the program scan. Output Q cannot be used to re-trigger the instruction because IN is edge triggered.
|
Status | Output | CIPSTATUS | The instruction block status. When an MSG is triggered or re-triggered, all elements inside Status are reset. The Status output is defined in CIPSTATUS data type. |
ResLength | Output | UINT | CIP message response data length: 0–490. When an MSG is triggered, or re-triggered, ResLength is reset to 0. |
MSG_CIPGENERIC examples
MSG_CIPGENERIC function block diagram example

MSG_CIPGENERIC ladder diagram example

MSG_CIPGENERIC structured text example

Provide Feedback