Message execution timing diagram (PCCC configuration error)

The following table describes the message conditions and bit status for each execution step identified in the timing diagram when a PCCC configuration error occurs during execution.
Message conditions and bit status when a PCCC configuration error occurs
Step
Message Description
Bit Status
1
Rung condition goes TRUE. Message execution is enabled.
EN bit is set.
2
Message buffer is acquired.
EW bit is set.
3
Invalid elements exist in PCCCCfg.
ER bit is set to 1 before ST bit is set to 1.
EW and ST bits do not change.
4
As rung condition goes FALSE.
EN, EW, and ER bits are cleared.

Error condition diagram

Error condition when changing the number of elements in PCCCCfg to an invalid number 17
Diagram showing error condition when changing the number of elements in PCCCCfg to an invalid number 17
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal