Embedded communication channels
The
Micro820
L20E and Micro850
L50E controllers have
the following additional embedded communication channels:- A non-isolated RS-232/485 combo port
- A non-isolated USB programming port (Micro850L50E only)
- An RJ-45 Ethernet port
Provide Feedback