TTABLE (truth table)
The TTABLE instruction provides the value of the output based on the combination of inputs. If the value is 0xABCD and In3 through In0 corresponds to the number 7, then TTABLE is the value of bit 7 in the table (which is 1). The least significant bit in the table is bit 0.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.TTABLE

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Table | Input | UINT | Truth table of BOOLEAN function. |
IN0 | Input | BOOL | Any BOOL input value. |
IN1 | Input | BOOL | Any BOOL input value. |
IN2 | Input | BOOL | Any BOOL input value. |
IN3 | Input | BOOL | Any BOOL input value. |
TTABLE | Output | BOOL | The value of the output according to the combination of inputs. |
TTABLE input combinations
The TTABLE instruction has four inputs, and therefore 16 combinations. These combinations are found in a truth table; for each combination, the output value can be adjusted. The number of configurable combinations depends on the number of inputs connected to the function.
Number | In3 | In2 | In1 | In0 |
|---|---|---|---|---|
1 | 0 | 0 | 0 | 0 |
2 | 0 | 0 | 0 | 1 |
3 | 0 | 0 | 1 | 0 |
4 | 0 | 1 | 0 | 0 |
5 | 0 | 1 | 0 | 1 |
6 | 0 | 1 | 1 | 0 |
7 | 0 | 1 | 1 | 1 |
8 | 1 | 0 | 0 | 0 |
9 | 1 | 0 | 0 | 1 |
10 | 1 | 0 | 1 | 0 |
11 | 1 | 0 | 1 | 1 |
12 | 1 | 1 | 0 | 0 |
13 | 1 | 1 | 0 | 1 |
14 | 1 | 1 | 1 | 0 |
15 | 1 | 1 | 1 | 1 |
TTABLE examples
TTABLE function block diagram example

TTABLE ladder diagram example

TTABLE structured text example

Results

Provide Feedback