RS (reset/set)

The RS instruction resets or sets the dominant (highest priority when determining instruction behavior) bistable.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
RS
RS
RS parameters
Parameter
Parameter Type
Data Type
Description
SET
Input
BOOL
TRUE: Sets Q1 to TRUE.
RESET1
Input
BOOL
TRUE: Sets Q1 to FALSE (dominant).
Q1
Output
BOOL
Boolean memory state.

RS examples

RS function block diagram example
RS function block diagram example
RS ladder diagram example
RS ladder diagram example
RS structured text example
RS structured text example
(* ST Equivalence: RS1 is an instance of a RS block *) RS1(start_cmd, (stop_cmd OR alarm)); command := RS1.Q1;
Results
Results
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal