AND

The AND instruction performs a Boolean AND operation between two or more values. It can be used as and symbol.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
AND
AND
AND parameters
Parameter
Parameter Type
Data Type
Description
i1
Input
BOOL
Value in Boolean data type.
i2
Input
BOOL
Value in Boolean data type.
o1
Output
BOOL
Result of the Boolean AND operation of the input values.

AND examples

AND function block program example
AND function block program example
AND ladder diagram program example
AND ladder diagram program example
(* ST equivalence: *) bo10 := bi101 AND NOT (bi102); bo5 := (bi51 AND bi52) AND bi53;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal