SCALER (scale)
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.SCALER

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | Instruction block enable.
Applies only to ladder diagram programs. |
Input | Input | REAL | Input signal. Input is not limited by InputMin and InputMax. To limit Input, a LIM instruction is needed to condition Input before it's entered to the SCALER instruction. |
InputMin | Input | REAL | Determine the slope and offset value. |
InputMax | Input | REAL | Determine the slope and offset value. |
OutputMin | Input | REAL | Determine the slope and offset value. |
OutputMax | Input | REAL | Determine the slope and offset value. |
Output | Output | REAL | Scaled Output. Output is not clamped between OutputMin and OutputMax. |
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
SCALER examples
SCALER function block diagram example

SCALER ladder diagram example

SCALER structured text example

(* ST equivalence: SCALER1 is an instance of SCALER block *) SCALER1(Signal_In, 4.0, 20.0 , 0.0 , 150.0 ) ; Out_Temp := SCALER1.Output ;
Results

Provide Feedback